Post Go back to editing

AdiCmdServerClient with custom FPGA board and custom AD9375 board

Hello All,

As a demo, I made a custom AD9375 board working with the Xilinx ZC706 board using ADI TES SD-CARD. I am using Matlab (custom GUI) and AdiCmdServerClient to configure, load and read signal and setup DPD. Everything works well.

For my next demo, I designed a custom FPGA board using a Zynq (same type as ZC706). I modified the ADi FPGA design to fit the new hardware.  Compilation works well and I am able to run simple applications.

In order to re-use my Matlab GUI/code with my custom FPGA Board, I would need to use the API with AdiCmdServerClient and generate my own "TES SDCARD". Could you share the code using AdiCmdServerClient so I can generate my proper boot image? Or do I have to redo everything based on your No-OS example and an LWIP application?

Thank you for your support.

Regards, 

Chris



?
[edited by: Chris449 at 10:43 AM (GMT 0) on 27 Aug 2019]
Parents
  • Hi,

    I'm trying to use ADRV9009 working with ZC706 to receive data on MATLAB. But there is a problem that I can't use AdiCmdSeverClient.dll because I can't find the head doc. Besides, I can't find any reference except the guides in the official web and I even don't know which function in Matlab is used to read the signal. Could you give me some advice?

    Thank you for your support.

    Yours,

    Selina

Reply
  • Hi,

    I'm trying to use ADRV9009 working with ZC706 to receive data on MATLAB. But there is a problem that I can't use AdiCmdSeverClient.dll because I can't find the head doc. Besides, I can't find any reference except the guides in the official web and I even don't know which function in Matlab is used to read the signal. Could you give me some advice?

    Thank you for your support.

    Yours,

    Selina

Children
No Data