Hello All,
As a demo, I made a custom AD9375 board working with the Xilinx ZC706 board using ADI TES SD-CARD. I am using Matlab (custom GUI) and AdiCmdServerClient to configure, load and read signal and setup DPD. Everything works well.
For my next demo, I designed a custom FPGA board using a Zynq (same type as ZC706). I modified the ADi FPGA design to fit the new hardware. Compilation works well and I am able to run simple applications.
In order to re-use my Matlab GUI/code with my custom FPGA Board, I would need to use the API with AdiCmdServerClient and generate my own "TES SDCARD". Could you share the code using AdiCmdServerClient so I can generate my proper boot image? Or do I have to redo everything based on your No-OS example and an LWIP application?
Thank you for your support.
Regards,
Chris
?
[edited by: Chris449 at 10:43 AM (GMT 0) on 27 Aug 2019]