Post Go back to editing

Sync toggling on logic device JESD204B TX to JESD204B RX on DAC side.

Thread Summary

The user is experiencing issues with the AD9082 device where the SYNC0OUTB± signal is toggling, indicating potential problems during the Initial Lane Synchronization (ILS) phase. The final answer suggests checking for SYSREF mismatch, lane clock/reference clock issues, and ensuring proper SYSREF alignment with the Device Clock. The user should also verify that the test setup follows the AD9081/AD9082 Software Development User Guide (UG-1578) and JESD HDL driver recommendations.
AI Generated Content
Category: Hardware
Product Number: AD9082

Hi, 

I am working with AD9082 device, when trying to link up between logic device JESD204B TX to JESD204B RX on DAC side the SYNC0OUTB+- from DAC to logic device is toggling, so we not sure wether we are getting link up or not. We are operating on 10Gbps lane rate and using UC23 testcase in the API for this device. To check the device state, we tried to read some of the monitoring and IRQ flag registers but we are getting 0x00 on them.

all these registers are in zero state. So we are not sure wether the sync is toggling as an indication of ILS stage or it is an idication of BD, NIT error on the serdes link. We read the BD, NIT counter, its value is also coming to be zero. 

So we need your help in this issue. 

  • HI  

    The SYNC0OUTB± signal toggling is symptomatic of the Initial Lane Synchronization (ILS) phase—that is, the link is attempting to establish itself and generate SYNC~ toggles to align code groups (CGS stage).

    Common problems could include:

    1. SYSREF mismatch or not properly captured for link start-up. SYSREF must align with Device Clock.
    2. Lane clock/reference clock issues—unsuitable PLL/CPLL not locking.

    We provide comprehensive guide—check “SYSREF captured: Yes” and “SYSREF alignment error: No”—these are key to diagnosing link states. Troubleshooting JESD204B Tx links [Analog Devices Wiki]

    The UC23 test sequence must or any 204B usecase must follow the same:

    • Trigger SYSREF
    • Enable link state machine monitoring
    • Poll status bits for CGS, ILS, IFS stages
    • If IRQ or monitor registers remain zero, it may indicate the API hasn't been instructed to enable monitoring or hasn't reached the state to begin counting. Ensure the test setup follows the Reference Manual UG-1578 and JESD HDL driver recommendations. AD9081/AD9082 Software Development User Guide, UG-1578 (Rev. A)

    Regards,

    SJ

  • Hi

    Thanks for the response ! 

    With the register page change we are now able to read the registers. Its show 3E on each lane that means we are getting into data phase. 

    We have one more issue, on the ADC side. On JESD RX in FPGA we are getting into data phase but once we get into data phase we starts to get disparity errors. So we are not sure what could be the reason because if its due to signal integrity issue it should have come during link up also. We are using UC 8 for ADC testing, we modified this testcase to single link from dual link and also changed the resolution (N) to 16 instead of 12. I am attaching the APIs log for more reference if that could help. ad9082_app (5).log