Post Go back to editing

AD9082-FMCA-EBZ Evaluation Board

Category: Datasheet/Specs
Product Number: AD9082-FMCA-EBZ

In AD9082-FMCA-EBZ Evaluation Board design, it includes AD9082BBPZ-4D-4AC which has ADC0_FD0, ADC0_FD1, ADC1_FD0, ADC1_FD1, ADC2_FD0, ADC2_FD1, ADC3_FD0, ADC3_FD1 pins.
In my design, I use AD9082BBPZ-4D-2AC which has ADC0_SMON0, ADC0_SMON1, ADC1_SMON0, ADC1_SMON1, ADC0_FD0, ADC0_FD1, ADC1_FD0, ADC1_FD1 pins.
Which pin corresponds to which pin?

Top Replies

  • FormerMember
    FormerMember
Sep 27, 2023 +1 verified

Hello,

Agree that naming convention used for pinout of device and schematic differ. 

Pinout (shown below) for the AD9082 can be found in the AD9082 datasheet.  The relevant  FMCA-EVB schematic screen shots…

Moving this over to the MxFE support forum

  • Hello,

    Agree that naming convention used for pinout of device and schematic differ. 

    Pinout (shown below) for the AD9082 can be found in the AD9082 datasheet.  The relevant  FMCA-EVB schematic screen shots are shown below showing how these pins are mapped on EVB to test points so that their state can be observed.