Post Go back to editing

AD9081 connecting DVDD1 and DVDD1_RT

Category: Datasheet/Specs
Product Number: AD9081
Software Version: N/A

I am designing the power tree for the AD9081, and there is a note on Pg 209 of the user guide (Rev0) that says this

I have other 1V rails not going to the AD9081 that I want to consolidate as much as possible. Which of the 2 rails is expected to have transient loads - DVDD1_RT or DVDD1? It's not clear what "it" is referring to in the highlighted sentence.

Also, how big is the current draw in these transients? 

Parents
  • FormerMember
    FormerMember
on Jul 15, 2022 10:04 AM
0

Hello,

DVDD1 draws the most current as shown in AD9081 power specification table and its transient load is based on the devices digital path configuration and clock rate.  One can refer to UG-1578 for different use case scenarios showing power consumption for each case.



Reply
  • FormerMember
    FormerMember
on Jul 15, 2022 10:04 AM
0

Hello,

DVDD1 draws the most current as shown in AD9081 power specification table and its transient load is based on the devices digital path configuration and clock rate.  One can refer to UG-1578 for different use case scenarios showing power consumption for each case.



Children