Post Go back to editing

Using Direct Clock on AD9081

Category: Software
Product Number: AD9081

Hello,

We would like to use AD9081 Direct Clock. (12GHz)

The datasheet says 0 to 6 dBm range when Direct RF input.

ez.analog.com/.../using-an-external-clock-with-ad9081-fmca-ebz

However, when we tried it, we found that it works only when we input higher power like the answer above.

(12GHz, 15 dBm or more , Source : Keysight E8257D)

When input below 9.5 GHz, it operates below 6 dBm.

Is it okay to use Direct CLK input at 12GHz with such a high input?

If not, is there anything I need to set up?

Thank you!

on Jul 14, 2022 9:43 AM
+1

Hello,

Besides cable losses from RF generator, the frequency response of the clock input path (SMA to clock input) also rolls off significantly at 12 GHz thus requiring such a high drive level to overcome the losses so 13 dBm operation of RF generator is fine.