Post Go back to editing

Usecase for bypassing the DDC in Full Bandwidth mode for AD9082.

Category: Software
Product Number: AD9082, VCU118
Software Version: api v1.2.2 commit 5b813df for ad9082

I am using VCU118 board + AD9082 with setup as shown in link wiki.analog.com/.../microblaze but with AD9082 board.

The aim is to bring up the two ADC of 9082 for 2GHz bandwidth and transmit the sampled data onto JESD204C.

I am referring to UG1578 and API (api v1.2.2 commit 5b813df for ad9082) for my development.

I am able to configure my setup for UC22.

The following are the requirements for my use case:

a) I want to enable my both ADC as per below figure:

b) DAC should not be enabled as I am not using it.

c) ADC Bandwidth should be 2GHz.

d) JESD204C to be used.

Kindly provide me the use case number to use to in uc_settings.c to meet the above requirement.

If use case is not readily available, then please provide the details to be populated in variables of uc_settings.c for my use case.

Parents Reply Children
No Data