Post Go back to editing

Looking for the MxFE sample product supporting 20GS/s

our project is to develope the system to support  data rate of 100 Gbps and need to have DACs/ADCs as fast as 20 GS/s

Might if Analog Devices is now developing the MxFE product supporting faster than AD9082?

and want to know when it is available. 

is there any way to raise the sampling speed using the AD9082 to the 20 GS/s? 

Regards, 

H.S. Kang

Parents
  • FormerMember
    FormerMember
on Jan 25, 2022 3:40 PM
0

Unfortunately the AD9082 can not support more than 6 GSPS ADC operation and 12 GSPS DAC operation.   
Considering the rapid advancements being made in high speed ADC and DAC technology, perhaps a 20 GSPS capable DAC and ADC with 10+ bit resolution will exist in a few years.

  • Reply Children
    No Data