Post Go back to editing

Temperature testing with AD9081/2 eval boards and ADS9?

I am interested in running some temperature testing at hot and cold with the AD9081 eval board (EVAL-AD9081) and the ADS9. I didn't see any documentation listing out the absolute max of the eval board and ADS9 -- are the temperature extremes limited by the AD9081 and FPGA on the ADS9? Are there any suggestions from ADI to follow?

Top Replies

  • FormerMember
    FormerMember
May 12, 2021 +1 verified

Hello,

Both boards were designed to operate around ambient temperature hence putting boards in a temperature chamber is not an option.  

A crude way of 0perating near the higher end of the die temperature…