Question:
I want to change the channel frequency quickly for a frequency hopping application using the ADF7024. How do I ensure the fastest possible frequency hop between channels?
---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Answer:
To change the channel frequency the host processor just needs to update the RADIO_CHANNEL_FREQ_X registers (address 0x109, 0x10A and 0x10B).
The host processor can write to these registers in PHY_OFF, PHY_ON, PHY_RX or PHY_TX. The new frequency doesn't get applied until a CMD_PHY_RX or CMD_PHY_TX is issued. Note there is no requirement to issue the CMD_CONFIG_DEV command after changing the RADIO_CHANNEL_FREQ_X registers.
So, as an example, if the ADF7024 is in PHY_RX and needs to go to PHY_RX on a new channel frequency the host processor should follow these steps:
- Write to registers 0x109, 0x10A and 0x10B sequentially using SPI_MEM_WR.
- Issue CMD_PHY_RX (i.e. 0xB2). The transition from PHY_RX (on previous channel frequency) to PHY_RX (on new channel frequency) takes 339.5us typically. (Refer to the ADF7024 Reference Manual and the state transition timing for more information on the timing)
This FAQ was generated from the following discussion: Change channel frequency quickly for a frequency hopping application using ADF7024