Hello everyone. I am working with the adrv9026 board. The input signal before reaching the adrv9026 will go through an Up Down Converter (gain about 30dB, Noise Figure about 4dB) to convert to intermediate frequency.
When I increase the RX gain from -12 to 0 dB on the ADRV9026, the noise floor will change from -91dBFS to -85 dBFS.
If I do not use the Up Down Converter, the ADRV9026 output noise floor is always -91dBFS even when changing the RX gain of the ADRV9026.
Can someone tell me why the noise floor is changed when installing the Up Down Converter before ADRV9026?
Thank you very much.