Post Go back to editing

Adf7023 rate problem

Thread Summary

The user inquired about configuring ADF7023 for a 300 kbps data rate, having previously succeeded with 100 kbps. The engineer recommended increasing the preamble to at least 24 bits (AFC Off, AGC Lock on Sync Word) or 64 bits (AFC On, AFC and AGC Lock on Preamble Detection) and using a frequency deviation of 75 kHz and an IF filter bandwidth of 300 kHz.
AI Generated Content

Hello .I would like to ask about the 300K rate configuration of ADF7023. I have already configured the rate of 100K before, but failed to configure the rate of 300K all the time. Therefore, I would like to ask, what are the requirements and matters needing attention for the 300K rate configuration of ADF7023? thank you