Post Go back to editing

ADF7020 continuous spurious output in rx mode, even when no carrier is present

Thread Summary

The user is experiencing a continuous stream of spurious random bits from the ADF7020 in RX mode, even without a carrier, and the synch word does not effectively mitigate this issue. The final answer indicates that questions about ADF7020 should be directed to the local sales organization for further support. No specific configuration settings to address the spurious output were provided.
AI Generated Content

Hello

I am working with the ADF7020, and notice that while in RX mode, the chip seems to output a continuous stream of spurious random bits, even in the complete absence of any carrier. Further, using the synch word helps a little, but there is enough randomness in this spurious data that it very frequently matches a synch word, so even using a synch word does not mitigate this. This occurs with both the linear FSK domodulator setting as well as with the correlator setting.

I was hoping to find some configuration setting that allows me to specify something like a minimum RSSI level below which it would not try to demodulate the input, but there does not seem to be anything like this.

What I would have hoped for would be that when there is no input there should be no output. I am using FSK. I'd have expected only to see a mark when the frequency corresponding to a mark is present, and a space only when the corresponding frequency is present.

Is it the expected behaviour to output a continuous stream of output when there is no carrier present?

If so, does anyone have any suggestions on how to deal with this? Again, even using a synch word does not address this because there are spurious occurrances of the synch word within the output stream.

Thanks much

Thread Notes