Post Go back to editing

ADF7021-N,RSSI level always 0.Where is my error?

Thread Summary

The user is unable to read the RSSI level on an ADF7021-N transceiver when controlled by a microcontroller, despite correct VDD, Product ID, and external ADC readings. The RSSI always reads 0x500, and the RSSI_Ready signal is always high. The final answer indicates that such questions should be directed to the local sales organization, as they are not handled on EngineerZone.
AI Generated Content

Hi to everybody in this forum,

thanks in advance just for reading this

My firmware is not able to read RSSI level on ADF7021-N mounted on a specific board

The board itself can be connected to the Eval board,and in this case RSSI can be read,

It is pretty correct,i.e -60dBm RSSI vs -59 dBm on a very good spectrum analyzer.

So i can guess that my hardware  works fine.

If i control the ADF7021 by means of a uC i can succesfully set the Tx frequency,i  have correct readback of VDD,Product Id(0x2111),external ADC IN but RSSI remains 0x500..

To have something different i have to let ADC disabled in register 8:I this case i have RSSI=0x52F ,changing signal level has not effect.

I use the EVB as a Tx,generating  a modulated signal,say 100MHz at2,4Kbps 1010 GFSK.

The Rx is my bord,

i set at 170Mhz Rx mode(synth dividers calculated 100KHz lower,169.90 Mhz), MUXOUT set to digital lock,i wait for it going high(in Tx it works)

then i perform the readback in the following steps

1)ADC Enable setting bit 8 of register 8   (0x108)

2)Setting value to write in Readback setup register :Readback for ADC out and ADC converting RSSI,Readback enabled

3)I write the above value(0x147) in Register 7 ,Readback Setup Register

4)I set register 0 to have RSSI_Ready  signalled on MUX_OUT ,

5)I wait until RSS_ Ready is high,but it it looks always high,..why?

6)I perform the Readback in 18 clock cycles

7)I turn off ADC

Thanks again for your attention

Diego


Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.