Post Go back to editing

ADF7021 Daughter board ADF7021DBZ5

Thread Summary

The user inquired about the necessary components to transmit at 144 MHz using the ADF7021DBZ5 daughter board, which comes with a 19.680 MHz XTAL. The final answer from the Analog Devices support team indicated that the question was closed and assumed answered, without specifying the required components. The application note AN-859 provides component details for the 140-150 MHz band, but it uses an 11.0592 MHz XTAL, which differs from the board's 19.680 MHz XTAL.
AI Generated Content

Hi,

I have this daughter board (ADF7021DBZ5) which i will stream to 144 MHz, then my question is, which components I need on this board to transmit at the desired frequency?, Since this board does not come with the necessary components to transmit.

In the application note AN-859 there are a components of the band 140-150 MHz, but on page 10 is the use of an XTAL of 11.0592 MHZ and ADF7021DBZ5 board comes already connected to 19.680 MHz XTAL.

So my question is: which components they need connect on this card to transmit a 144 MHz to 19,680 MHz XTAL?

Thread Notes