Hello,
Does ADF7020 has software reference manual, just like UG-1002 for ADF7030-1. Or could you advice how to set the state of interface such as RXCLK&RxDATA.
Edit Notes
none[edited by: karo at 2:54 AM (GMT 0) on 26 Mar 2019]
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADF7020
Not Recommended for New Designs
The ADF7020 is a low power, low-IF transceiver designed for operation in the license-free ISM bands at 433MHz, 868MHz and 915MHz. It is suitable for circuit...
Datasheet
ADF7020 on Analog.com
ADF7030-1
Not Recommended for New Designs
The ADF7030-1 is a fully integrated, radio transceiver achieving high performance at very low power. The ADF7030-1 is ideally suited for applications that...
Datasheet
ADF7030-1 on Analog.com
Hello,
Does ADF7020 has software reference manual, just like UG-1002 for ADF7030-1. Or could you advice how to set the state of interface such as RXCLK&RxDATA.
Hi,
You may refer to the user guide (https://www.analog.com/media/en/technical-documentation/data-sheets/ADF7020.pdf) regarding this. "Serial interface allows the user to program the fourteen 32-bit registers using a 3-wire interface (SCLK, SDATA, and SLE)" as the user guide says.
Please not, however, that ADF7020 is already not support. We recommend that you either evaluate ADF7023(https://www.analog.com/media/en/technical-documentation/data-sheets/ADF7023.pdf ) or ADF7030-1(https://www.analog.com/media/en/technical-documentation/data-sheets/adf7030-1.pdf ) for your application.