Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers
    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers

    Introduction to Industrial I/O, libIIO, and Python software tools

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Evaluating Power Supplies with Different Compensation Settings

    Evaluating Power Supplies with Different Compensation Settings

EngineerZone
EngineerZone
Support AD9361/AD9363/AD9364
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Support AD9361/AD9363/AD9364
  • RF & Microwave
  • RF Transceivers
  • Support AD9361/AD9363/AD9364
  • Cancel
Support AD9361/AD9363/AD9364
Documents AD936x Built in Self Test (BIST)
  • Q&A
  • Files
  • Docs/ FAQs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +AD9361: FAQ
  • +AD9363: FAQ
  • -AD936x: FAQ
    • AD936x Built in Self Test (BIST)
    • AD936x digital interface capacitive load drive in CMOS mode
    • AD936x documentation changes
    • AD936x Local Oscillator [LO]
    • AD936x maximum Rx digital path data rates
    • AD936x Rx ADC basic operation and output rates
    • AD936x Temperature sensor
    • AD936x_DCOFFSET_ISSUE
    • Transmit Power monitor (TPM) AD936x
  • +Gain Tables: FAQ

AD936x Built in Self Test (BIST)

BIST Signal Generator

AD9361 and AD9364 have an internal signal generator which can be used to inject a signal into either the output of the Tx data port or the input of the Rx data port. This is useful when testing the connectivity of the Rx data port or the Tx RF output. It is a useful tool when debugging effects in the Tx chain of the AD9361. It allows the user to rule out the Tx data port as the source of issues, as it allows the user to generate a signal and inject it at the output of the Tx data port. Please see the attached document for more details.

Attachments:
AD9361BISTFAQ.pdf
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • RE: AD9361 Loop Test , Repeater Application
    ADIApproved
    The AD9361 has an internal signal generator which can be used to inject a signal into either the output of the Tx data port or the input of the Rx data port. This is useful when testing the connectivity...
  • RE: AD9361 Loop Test , Repeater Application
    ADIApproved
    The AD9361 has built in features that allow the user to test the data port and RF functionality of the chip. The features comprise data loopback mode, where data received through the Tx data port is fed...
  • RE: Data Port Loop Test for AD9364
    ADIApproved
    I would suggest using the internal BIST generator to perform the test first. By using the BIST generator you can test the Tx signal chain (observe Tx output on a spectrum analyzer) and observe data at...
 
Related Content
  • RE: AD9361 Loop Test , Repeater Application
    ADIApproved
    The AD9361 has an internal signal generator which can be used to inject a signal into either the output of the Tx data port or the input of the Rx data port. This is useful when testing the connectivity...
  • RE: AD9361 Loop Test , Repeater Application
    ADIApproved
    The AD9361 has built in features that allow the user to test the data port and RF functionality of the chip. The features comprise data loopback mode, where data received through the Tx data port is fed...
  • RE: Data Port Loop Test for AD9364
    ADIApproved
    I would suggest using the internal BIST generator to perform the test first. By using the BIST generator you can test the Tx signal chain (observe Tx output on a spectrum analyzer) and observe data at...