Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
Support AD9361/AD9363/AD9364
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Support AD9361/AD9363/AD9364
  • RF & Microwave
  • RF Transceivers
  • Support AD9361/AD9363/AD9364
  • Cancel
Support AD9361/AD9363/AD9364
Documents AD936x Rx ADC basic operation and output rates
  • Q&A
  • Files
  • Docs/ FAQs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +AD9361: FAQ
  • +AD9363: FAQ
  • -AD936x: FAQ
    • AD936x Built in Self Test (BIST)
    • AD936x digital interface capacitive load drive in CMOS mode
    • AD936x documentation changes
    • AD936x Local Oscillator [LO]
    • AD936x maximum Rx digital path data rates
    • AD936x Rx ADC basic operation and output rates
    • AD936x Temperature sensor
    • AD936x_DCOFFSET_ISSUE
    • Transmit Power monitor (TPM) AD936x
  • +Gain Tables: FAQ

AD936x Rx ADC basic operation and output rates

The Rx ADC used in AD936x devices is a highly oversampled sigma-delta modulator (SDM) with an output ranging from +4 to -4. A particular ADC output sample does not necessarily represent the input signal at a particular time. Rather, a positive value indicates that the input signal is more positive since the last sample and a negative value indicates that the input signal is more negative since the last sample. Note that since the ADC is highly oversampled, the ADC clock is much faster than the receive sample rate. Decimating and low pass filtering result in digital samples that represent the analog signal.

The ADC minimum and maximum operating output data rates are 25MHz and 640MHz respectively. The min and max rate need to be used as constraints for Rx digital data path design.