Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
Support AD9361/AD9363/AD9364
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Support AD9361/AD9363/AD9364
  • RF & Microwave
  • RF Transceivers
  • Support AD9361/AD9363/AD9364
  • Cancel
Support AD9361/AD9363/AD9364
Documents AD936x Temperature sensor
  • Q&A
  • Files
  • Docs/ FAQs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +AD9361: FAQ
  • +AD9363: FAQ
  • -AD936x: FAQ
    • AD936x Built in Self Test (BIST)
    • AD936x digital interface capacitive load drive in CMOS mode
    • AD936x documentation changes
    • AD936x Local Oscillator [LO]
    • AD936x maximum Rx digital path data rates
    • AD936x Rx ADC basic operation and output rates
    • AD936x Temperature sensor
    • AD936x_DCOFFSET_ISSUE
    • Transmit Power monitor (TPM) AD936x
  • +Gain Tables: FAQ

AD936x Temperature sensor

AD9361 / AD9363 / AD9364 temperature sensor.

The internal temperature sensor value can be read using the Auxiliary ADC (AuxADC) via SPI. The AuxADC needs to be configured using the ad9361_auxadc_setup function to configure the part in temperature sensor mode.  Then use the ad9361_get_temp function to do a reading. To prevent issues with competing functions interfering with each other, it is recommended to disable the Auxiliary ADC pin‐measurement function when using the temperature sensor function.

 

The temperature sensor has inaccuracies and even with a onetime calibration the sensor is typically not useful for accurate measurements.

Details captured in attached document.

Attachments:
AD936xTemperaturesensor.pdf
Tags: temperature sensors ad9361 temperature sensor
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • RE: AuxADC filtering
    srimoyi
    Can you please explain in details about your requirement? Are you planning to measure the voltage on the AUXADC pin or are you looking for only internal temperature sensor measurement? The temperature...
  • RE: How do I use the Temperature Sensor?
    ADIApproved
    If you need to know the temperature of the AD9361 itself, the temperature sensor is a great way to get this information with simple SPI reads. However, if the main goal is to measure system temperature...
  • RE: internal temp sensor ad7794
    MaryMc
    Hello Mircea, firstly, there will be some variation in the codes generated by the AD7794 when the internal temp sensor is used. An external calibration is needed to correct for this. When the temperature...
 
Related Content
  • RE: AuxADC filtering
    srimoyi
    Can you please explain in details about your requirement? Are you planning to measure the voltage on the AUXADC pin or are you looking for only internal temperature sensor measurement? The temperature...
  • RE: How do I use the Temperature Sensor?
    ADIApproved
    If you need to know the temperature of the AD9361 itself, the temperature sensor is a great way to get this information with simple SPI reads. However, if the main goal is to measure system temperature...
  • RE: internal temp sensor ad7794
    MaryMc
    Hello Mircea, firstly, there will be some variation in the codes generated by the AD7794 when the internal temp sensor is used. An external calibration is needed to correct for this. When the temperature...