Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    Latest Webinars

    • Fast-Track Certification: Leveraging IC Safety App Notes for Functional Safety Designs
    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
    • Design Smarter with Compact, Low-Power Precision Current Source Signal Chains
    • Power Management Fundamentals II Session 6: Key Layout Considerations for Power
    View All Webinars
  • Community Hub

    Challenge Yourself!

      World Engineering Day Quiz!

      A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How many squares, defined...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    Highlighted Blogs

    The New Industrial Robotics Era: Why Innovation Is Compounding

    By Tracey Johnson & Margaret Naughton Imagine a robot stepping out of a safety cage, not to perform a single preprogrammed motion, but to work alongside...

     

    Reimagining Power for AI: Shaping the Future of AI Acceleration: Part 3 of 3

    It’s time to look at the next wave: vertical power delivery and the relentless Analog Devices (ADI) innovation that makes it possible. If you’ve joined...

    Latest Blogs

    • Driving Capacitive Loads Like A Pro: Part 3 of 3
    • Community Spotlight: Meet Akila
    • A Systematic Checklist for RF Transceiver Testing
    • Breaking the Link: Smart Feedback Techniques for Isolated SMPS Regulation: Part 4 of 4
    • Good Marketing Buzz, But How Do I Start?
    Read All Blogs

    ADI Blogs

    • EZ Spotlight
    • The Engineering Mind
  • ContentZone

    Visit ContentZone

    ContentZone

    Technical articles. Blogs. Videos. Your ADI content, all in one place.

    View ContentZone

    Featured Content

    Featured Content Title

    Blurb About Content

    View Content By Industry

    • Aerospace and Defense Systems
    • Automotive Solutions
    • Consumer Technology Solutions
    • Data Center Solutions
    • Energy Solutions
    • Healthcare Solutions
    • Industrial Automation Technology Solutions
    • Instrumentation and Measurement Solutions
    • Intelligent Building Solutions
    • Wireless Communication Solutions

    View Content By Technology

    • A2B Audio Bus
    • ADI OtoSense Predictive Maintenance Solutions
    • Dynamic Speaker Management
    • Gallium Nitride (GaN) Technology
    • Gigabit Multimedia Serial Link (GMSL)
    • Industrial Vision
    • Power Solutions
    • Precision Technology
    • RF
    • Sensor Interfaces
    • SmartMesh
EngineerZone
EngineerZone
Support AD9361/AD9363/AD9364
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Support AD9361/AD9363/AD9364
  • RF & Microwave
  • RF Transceivers
  • Support AD9361/AD9363/AD9364
  • Cancel
Support AD9361/AD9363/AD9364
Documents Transmit Power monitor (TPM) AD936x
  • Q&A
  • Files
  • Docs/ FAQs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +AD9361: FAQ
  • +AD9363: FAQ
  • -AD936x: FAQ
    • AD936x Built in Self Test (BIST)
    • AD936x digital interface capacitive load drive in CMOS mode
    • AD936x documentation changes
    • AD936x Local Oscillator [LO]
    • AD936x maximum Rx digital path data rates
    • AD936x Rx ADC basic operation and output rates
    • AD936x Temperature sensor
    • AD936x_DCOFFSET_ISSUE
    • Transmit Power monitor (TPM) AD936x
  • +Gain Tables: FAQ

Transmit Power monitor (TPM) AD936x

Transmit Power Monitor (TPM) functionality - AD936x

The on-board transmit (TX) power monitor can be used as a power detector, enabling highly accurate TX power measurements in TDD mode. Maximum input power to TPM port is +4dBm and it has an accuracy of 1 dB. TPM functionality is described under ‘Tx Power monitor section’ in User Guide (UG-570).

 


TPM reuses RX circuitry, hence same is only useful in TDD mode. In TDD mode you cannot take the IQ data out using TPM port.  A few points to take care while using TPM port:

  • TX Mon DC Offset Cal is redundant, no need to execute
  • In TDD mode, bit 0x015[D2] (Dual Synth Mode) should be set HIGH. This allows the RX Synth and associated circuitry to stay high when needed for TPM
  • TX1 and TX2 Transmit Attenuation should be equal to avoid crosstalk

TPM Test mode. (I,Q data out using TPM port)

If the application is TDD, it is not possible to output TPM IQ data on the RX data port as the TDD state machine is overriding the 0x14[D7] bit and is not enabling the Rx port for data transmission. But this is possible in FDD mode, where both the data paths are enabled. Steps for doing this are:

  • Register 0x001[D6:D5] – set the Bits high.
  • Register 0x014 Bit D7 (Enable Rx Data Port) - needs to be set high.
  • Register 0x06E Bits D7 and D5 (TPM Enable) - needs to be set high.
  • Register 0x057 Bits D2 and D3  ( Analog Power Down Override) – needs to be cleared

TPM(TX RSSI t for FDD mode set Register 0x001[D6:D5] – set the Bits high

Tags: tpm ad9361 transmit power monitor ad9364
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • RE: Tx Monitor I/Q output
    PVALAVAN
    TPM Test mode. (I,Q data out using TPM port) If the application is TDD, it is not possible to output TPM IQ data on the RX data port as the TDD state machine is overriding the 0x14[D7] bit and is not...
  • RE: IIO Oscilloscope TX Power Monitoring (TPM)
    srimoyi
    TPM is mainly used in TDD mode. It can only be used in TX mode, when the RX path remains unused. Refer to the below document: Transmit Power monitor (TPM) AD936x
  • tpm
    tpm
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
 
Related Content
  • RE: Tx Monitor I/Q output
    PVALAVAN
    TPM Test mode. (I,Q data out using TPM port) If the application is TDD, it is not possible to output TPM IQ data on the RX data port as the TDD state machine is overriding the 0x14[D7] bit and is not...
  • RE: IIO Oscilloscope TX Power Monitoring (TPM)
    srimoyi
    TPM is mainly used in TDD mode. It can only be used in TX mode, when the RX path remains unused. Refer to the below document: Transmit Power monitor (TPM) AD936x
  • tpm
    tpm
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")