Post Go back to editing

Configuration for External LNA

I'm using AD9364 in Fast Attack AGC with Split table mode. We are also using an external LNA of 22dB gain and 2 variable gain amplifiers each of 19dB gain and variable attenuation of 0.5 to 31.5dB in steps of 0.5dB. Without using these amplifiers, My AGC settings works fine. If I want to use these front end module, how to configure my External LNA setting in AD9364 init? 

Just entering the settling time for all these front end module itself is enough or do I also need to modify the split gain table?

I'm using Split table mode.

Parents
  • The default peak overload wait time is fine for all applications until you are using an external LNA with bypass(low gain)mode.

    Yes if you add the LNA gain in the gain table then it will impact your AGC as in that case the total gain will change. There are two bits for external LNA gain control 0x026[bitsD6:D5] for RX1 and RX2.

    Since there is only one bit per RX you can vary the LNA gain between two levels (.i.e. the external LNA gain index can be either 0 or 1 and accordingly the gain can vary between two levels).

    Please refer the external LNA section in UG for more details.

  • Hi Srimoyi..i want to use external LNA in bypass mode, with AGC in fast attack mode in AD9361. So, do i need only increase peak overload wait time or anything else also must be updated..? if anything else must be updated..can u please specify what to?

  • Is external LNA present in your design? if not, no need to update the gain table and the default gain table can be used, so you don't need to update the threshold values.

    Please refer to the External LNA section of the user guide.

    Please open a new post if you have any questions and please don't add to the old posts.

Reply
  • Is external LNA present in your design? if not, no need to update the gain table and the default gain table can be used, so you don't need to update the threshold values.

    Please refer to the External LNA section of the user guide.

    Please open a new post if you have any questions and please don't add to the old posts.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.