AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiverâ„¢ designed for use in 3G and
4G base station applications....
Datasheet
AD9361 on Analog.com
Hi,
I would like to produce an AGC with an external LNA.
Should I calculate the values within the table to have a continuous gain when switching the external LNA (taking into account the external LNA)?
My external gain is about 36dB and the bypass mode -8dB, how can I use the 0x12c and 0x12d to express this (as they are limited to 31.5dB)?
Thanks,
Yossi
Hi Yossi,
Since your bypass gain is negative you would need to even further increase your high gain.
From the manual: "If the low gain value is negative then the Ext LNA High Gain should be offset by this amount and the Ext LNA Low Gain should be set to 0 (for example, high gain value = 15 dB, low gain value = −5 dB, program Ext LNA High Gain = 20 dB and Ext LNA Low Gain = 0 dB). This will prevent a step in the RSSI value when the external LNA goes from an on to an off condition."
I think the experts on the AD9361 design forum can give you better insights on how to handle this case.
-Michael
Moved to AD9361 Design Support.
-Michael
Hi Yossi,
From my experience the RSSI is not reported correctly when the external LNA is bypassed. See here - AD9364 RSSI issue
The 12C and 12D registers are used only for RSSI report, they do not affect the AGC operation. Your gain table should contain correct gain settings for LNA on and LNA bypass scenarios, in order to maintain linear AGC response.
Best regards,
Oleg.