AD9261 Reference Manual UG-570 contains following information:
"The Rx FIR has two options for its sample clock, either ADC_CLK or ADC_CLK/2"
How I can change this?
AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiver™ designed for use in 3G and
4G base station applications. Its...
Datasheet
AD9361 on Analog.com
AD9261
Not Recommended for New Designs
The AD9261 is a 16-bit analog-to-digital converter (ADC) based on a continuous time sigma-delta (S-?) architecture that achieves 86 dB of dynamic range...
Datasheet
AD9261 on Analog.com
AD9261 Reference Manual UG-570 contains following information:
"The Rx FIR has two options for its sample clock, either ADC_CLK or ADC_CLK/2"
How I can change this?
It is internally taken care depending on the TX and RX path rates and cannot be configured.