AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiverâ„¢ designed for use in 3G and
4G base station applications....
AD9361 on Analog.com
We have designed a circuit board with the AD9361 and see some unexpected noise floor shapes when receiving 54 MHz of bandwidth through the chip. All of the bandwidths were created using the Matlab AD9361 plug-in. Attached are two spectral views. The first uses a 40 MHz bandwidth and shows a reasonably flat noise floor. The second view uses the 54 MHz filter but the noise floor at each end rises up about 10 dB then starts to tail off. The noise floor on the transmit output for both the 40 MHz and 54 MHz bandwidth are flat.
Are these noise floor lobes due to the sigma-delta ADC? Is there some way to get rid of or reduce them? The 54 MHz bandwidth uses an ADC rate of 480 MHz and a final sample rate of 60 MHz (decimate by 8). We can't run the ADC at a higher rate without violating the max transfer rate between the AD9361 and our FPGA since we use FDD mode and all channels (RX1, RX2, TX1 and TX2).
Thanks,
It could be the filter response that you are seeing. Can you remove the input Rx signal, terminate the input and run it at max gain? This experiment should show the filter response and once it does you can try to correlate it with the shape you are seeing now.
I don't think it is the sigma delta ADC since you are running it a much greater rate than your bandwidth of interest. Sigma delta ADC does have noise transfer function that increases with frequency.
It could be the filter response that you are seeing. Can you remove the input Rx signal, terminate the input and run it at max gain? This experiment should show the filter response and once it does you can try to correlate it with the shape you are seeing now.
I don't think it is the sigma delta ADC since you are running it a much greater rate than your bandwidth of interest. Sigma delta ADC does have noise transfer function that increases with frequency.