Post Go back to editing

AD9364 CMOS input overshoot vs abs-max (-0.3 V / VDD_INTERFACE+0.3 V): transient allowance?

Thread Summary

The user asks if a few-ns overshoot beyond the AD9364's CMOS logic input abs-max (-0.3 V / VDD_INTERFACE+0.3 V) is acceptable when the clamp current remains within ±10 mA. The final answer confirms that some overshoot and undershoot are expected but should be minimized through proper drive strength and slew rate settings. For the CMOS interface, using DRIVE 4 SLEW SLOW or series resistors on the FPGA side is recommended to reduce overshoot.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD9364

TL;DR: board SI sims show ns-long overshoot on AD9364 CMOS logic inputs beyond the Table 11 abs-max (-0.3 V / VDD_INTERFACE+0.3 V), while the clamp current stays well below the +-10 mA rating. ADALM-PLUTO Rev D shows the same with the same method. Is this acceptable?

Setup: AD9364BBCZ, VDD_INTERFACE 1.8 V, CMOS interface, driven by Zynq-7010 LVCMOS18 (same topology as ADALM-PLUTO Rev D).

Sim (IBIS, PowerSI + SPDSIM, max corner):

  • Zynq DRIVE 12 (default): 14 of 23 inputs exceed; worst 2.62 V / -0.83 V; clamp current 1.9 / -3.6 mA.
  • Zynq DRIVE 4 SLEW SLOW: 3 of 23 exceed; worst -0.52 V.
  • ADALM-PLUTO Rev D, same method: all inputs exceed; worst 2.50 V / -0.74 V.

Questions:

  1. Is a few-ns overshoot beyond -0.3 V / VDD_INTERFACE+0.3 V acceptable when the input current stays within +-10 mA? Is there any duration rule?
  2. For the CMOS interface, do you recommend DRIVE 4 SLEW SLOW (or series resistors) on the FPGA side, or is the Pluto default considered safe?

Related: thread 594451 (static levels only). Thanks!

Parents
  • HI  

    I will try to answer this briefly. For interface lines carrying high-speed digital data, some amount of overshoot and undershoot during signal transitions is expected. The magnitude of these transients depends on the PCB interconnect characteristics, parasitic capacitance, device-pin capacitance, driver strength, signal edge rate, and interface speed. Such transient behavior is primarily a signal-integrity consideration, and excessive overshoot or undershoot should be minimized through appropriate drive-strength and slew-rate settings, PCB layout, and termination where necessary.


    Regards,
    SJ

Reply
  • HI  

    I will try to answer this briefly. For interface lines carrying high-speed digital data, some amount of overshoot and undershoot during signal transitions is expected. The magnitude of these transients depends on the PCB interconnect characteristics, parasitic capacitance, device-pin capacitance, driver strength, signal edge rate, and interface speed. Such transient behavior is primarily a signal-integrity consideration, and excessive overshoot or undershoot should be minimized through appropriate drive-strength and slew-rate settings, PCB layout, and termination where necessary.


    Regards,
    SJ

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.