Post Go back to editing

AD9364 VDD_GPO rising after the 1.3 V rails - acceptable? (same as ADALM-PLUTO Rev D)

Thread Summary

The user asks about the risks of VDD_GPO lagging the 1.3 V domain during power-up in an AD9364 design, similar to the Pluto Rev D setup. The final answer explains that this can cause abnormal internal currents due to active 1.3 V domain components while VDD_GPO is unpowered. ADI recommends following the standard power-up sequence: VDD_GPO, VDD_INT, then VDD_1P3/VDDAx. Holding RESETB low until VDD_GPO is up helps but does not eliminate the power-sequencing issue.
AI Generated Content
Category: Hardware

Hello, the AD9361 power FAQ (thread 80731) and UG-570 say VDD_GPO must rise as fast or faster than the 1.3 V supply domain. In our AD9364 design, VDD_GPO (2.7 V from an ADP151 LDO) is enabled by the open-drain power-good of the 1.3 V LDOs, so VDD_GPO only starts ramping after the 1.3 V rails are in regulation (we have not measured the delay yet). The ADALM-PLUTO Rev D does the same: its VDD_GPO is the 3.3 V rail from an ADM7160 whose EN is also driven by PG_1P3V.

1) What is the risk or failure mode if VDD_GPO lags the 1.3 V domain at power-up?

2) Is the Pluto Rev D arrangement considered acceptable by ADI?

3) Would holding RESETB low until VDD_GPO is up remove the concern?

Thank you.

Parents
  • HI  

    The standard recommendation to follow here for powering up AD936x family series. First power up VDD_GPO => VDD_INT => VDD_1P3/VDDAx. This sequence is clearly specified in AD9361 datasheet and user guide and request to follow as per the same. Please find below datasheet snippet.

    1) What is the risk or failure mode if VDD_GPO lags the 1.3 V domain at power-up?

    We don't have qualitative failure data to say exactly to maintain. The engineering concern is that portions of the AD9361/AD9364 powered from the 1.3 V domain can be active while the VDD_GPO domain is unpowered. That creates the possibility of internal bias/current paths between supply domains, potentially causing abnormal internal current during ramp. 

    2) Is the Pluto Rev D arrangement considered acceptable by ADI?

    In Pluto design, There may be implementation-specific factors, including ramp times and the actual duration/magnitude of the VDD_GPO-to-1.3 V differential, that ADI validated on Pluto. Therefore, for your AD9364 production design, I would not use Pluto alone as justification for departing from the published rule.

    3) Does holding RESETB low until VDD_GPO is established fix it?

    It helps considerably with startup-state integrity, but it does not remove the power-sequencing violation itself.

    Regards,

    SJ

Reply
  • HI  

    The standard recommendation to follow here for powering up AD936x family series. First power up VDD_GPO => VDD_INT => VDD_1P3/VDDAx. This sequence is clearly specified in AD9361 datasheet and user guide and request to follow as per the same. Please find below datasheet snippet.

    1) What is the risk or failure mode if VDD_GPO lags the 1.3 V domain at power-up?

    We don't have qualitative failure data to say exactly to maintain. The engineering concern is that portions of the AD9361/AD9364 powered from the 1.3 V domain can be active while the VDD_GPO domain is unpowered. That creates the possibility of internal bias/current paths between supply domains, potentially causing abnormal internal current during ramp. 

    2) Is the Pluto Rev D arrangement considered acceptable by ADI?

    In Pluto design, There may be implementation-specific factors, including ramp times and the actual duration/magnitude of the VDD_GPO-to-1.3 V differential, that ADI validated on Pluto. Therefore, for your AD9364 production design, I would not use Pluto alone as justification for departing from the published rule.

    3) Does holding RESETB low until VDD_GPO is established fix it?

    It helps considerably with startup-state integrity, but it does not remove the power-sequencing violation itself.

    Regards,

    SJ

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.