Post Go back to editing

Physical compatibility with zcu102

Thread Summary

The user encountered an issue with the AD9361 evaluation board FMCOMMS5 being too long to fit on the ZCU102 due to an inductor. The solution is to use FMC risers, specifically the Samtec VITA 57.1 FMC Extender Card, which provides the necessary clearance. The REF-228680-01 connector alone is not sufficient; it must be used with a riser/extender that includes both male and female connectors.
AI Generated Content
Category: Hardware
Product Number: AD9361

Hi, when mounting AD9361 evaluation board FMCOMMS5 with ZCU102 the length of the board is bigger than the space in zcu102. What should I do??

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.