Post Go back to editing

I need some help and suggestions regarding communication with MAX2223 and AD9364 using the MSP430F5529. I am trying to communicate with the MAX2223 IC through I²C and with the AD9364 through SPI, both using the MSP430F5529.

Thread Summary

The user is experiencing issues with I²C communication with the MAX2223 and SPI communication with the AD9364 using the MSP430F5529LP. The final answer suggests checking the SPI timing at 1MHz or lower and verifying SPI read/write operations to the scratch pad and device registers. The user should also ensure proper I²C address configuration and pull-up resistors for the MAX2223.
AI Generated Content
Category: Hardware
Product Number: MAX2223 IC

Hi Team,

I need some help and suggestions regarding communication with MAX2223 and AD9364 using the MSP430F5529LP.

I am trying to communicate with the MAX2223 IC through I²C and with the AD9364 through SPI, both using the MSP430F5529LP.

For the MAX2223, I configured it for a 7-bit I²C address by grounding Pin 28, but I am still unable to establish I²C communication.

I also tested SPI communication with the AD9364, but that is not working either.

Both the MAX2223 board and the AD9364 board are custom-designed boards. I have already checked the basic power supply and signal connections.

Could anyone please suggest what else I should verify? In particular, I would appreciate guidance on:

  • MAX2223 I²C address configuration and pull-up resistors 4.7 K ohms Provided for SDA and SCL.
  • MSP430F5529 I²C configuration
  • AD9364 SPI timing and connection requirements
  • Clock, reset, chip-select, and signal-level checks

Any suggestions for debugging these communication issues would be very helpful.

Thank you in advance.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.