Post Go back to editing

AD9364

Thread Summary

The user inquired about the input dynamic range and P1dB of the ADRV9364 evaluation board at 0dB and maximum gain. The receiver can handle inputs of -70dBm at high gain and 0-5dBm at low gain, with the P1dB and saturation limits of each stage (LNA, Mixer, ADC) determining the overall system limits.
AI Generated Content
Category: Hardware
Product Number: AD9364

what is the Input Dynamic Range of ADRV9364 evalution board and can you please tell about the P1dB (with 0dB Gain & max Gain)

  • HI  ,

    Typically, our Receiver can take input at high gain and low gain configurations as -70dBm and 0-5dBm respectively. As we have frontend attenuator before any Block in the receiver chain. Based on the gain table configuration your maximum input is determined.  

    Regards,

    SJ

  • The ADC is placed after the LNA and mixer in the signal chain. We need to determine the individual P1dB and saturation limits of each module.

    The signal chain is:

    RF Input → LNA → Mixer → ADC

    For each module, we need to identify its input and output P1dB levels, maximum allowable input power, and saturation or clipping limits. Based on the gain or conversion loss of each stage, the signal power at the output of one stage can be calculated and used as the input power to the next stage.

    The overall system limit is determined by the stage that reaches its compression or saturation limit first. For the ADC, the corresponding full-scale input or clipping level should also be considered.

    Therefore, the analysis should determine:

    • LNA input/output P1dB and saturation limits

    • Mixer input/output P1dB and saturation limits

    • ADC full-scale input and clipping limits

    • Signal power at each interface

    • Available power margin at each stage

    • Maximum allowable input signal for linear operation of the complete chain

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.