Post Go back to editing

AD9363 to AD9361 migration on PlutoSDR Rev D - 3 hardware questions

Thread Summary

The user is adapting the PlutoSDR Rev D design to use the AD9361BBCZ for dual receive operation. The final answer suggests referring to the FMCOMMS2 or FMCOMMS3 board schematics for 2.4GHz or wideband applications, respectively, to ensure proper component population and schematic changes. The AD9361 VDD_INTERFACE is on the 1V8 rail, and the user should verify power sequencing and timing requirements with the AD9361 datasheet.
AI Generated Content
Category: Hardware
Product Number: AD9361BBCZ, AD9361

I am adapting the PlutoSDR Rev D design (which uses AD9363ABCZ) to use the AD9361BBCZ instead, to enable the second receive chain. Both parts are BGA144-2 and I understand the footprint is the same. I have three hardware questions before updating the design.

Question 1 - Schematic changes beyond DNI population

The PlutoSDR Rev D schematic has T2, D9 and D10 marked DNI for the RX2A chain. I intend to populate these for full dual receive operation.

a) Beyond populating T2 (TCM1-63AX+ balun), D9 and D10 (ESD8472MUT5G), are there any other components that must be added or changed on the Rev D schematic to properly support the AD9361 RX2A chain?
b) Are there any resistor or capacitor values on the RX2A path that differ from the RX1A path on Rev D?
c) The Rev D wiki states the second Rx/Tx channel is not tested during production test. Is there any known hardware limitation on Rev D that affects RX2A performance with AD9361?

Question 2 - Full RX2A component population list

To confirm I have not missed anything, can you provide or confirm the complete list of components that must be populated on PlutoSDR Rev D to enable RX2A with AD9361? I have identified: T2, D9, D10. Are there any passive components on the RX2A supply line or matching network that are also DNI by default?

Question 3 - Power sequencing with Zynq-7020

I am also upgrading from Zynq-7010 to Zynq-7020. The Rev D power sequence is: 1V0 first, then 1V8, then 1V35. The AD9361 VDD_INTERFACE is on the 1V8 rail.

a) Does the AD9361 have any specific power sequencing requirement relative to VDD_INTERFACE and the core supply?
b) Is there any minimum time delay required between 1V0 stable and 1V8 enable?
c) Should AD9361 RESETB be held low until all supplies are stable, and if so which supply is the last to stabilise before RESETB can be released?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.