Hi,
Is it possible to configure the rx and tx baseband sampling rate differently, e.g. rx = 92.16 MSPS and tx = 102.4 MSPS?
Edit Notes
Typo[edited by: olegeorg at 11:27 AM (GMT -4) on 30 Jul 2026]
AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiverâ„¢ designed for use in 3G and
4G base station applications....
Datasheet
AD9361 on Analog.com
Hi,
Is it possible to configure the rx and tx baseband sampling rate differently, e.g. rx = 92.16 MSPS and tx = 102.4 MSPS?
Hi,
Ok, thanks for confirmation. Do analog device offer other RF transceiver chip(s) that have similar performances as AD9361, but support my sampling rates requirement.
Hi,
One Rx and Tx channel. I can use external LO if it is necesarry. Rx @305 MHZ and Tx @255 MHz. The sampling rate from the ADC to the FPGA must be 92.16 MSPS and the sample rate from the FPGA to the DAC must be 102.4 MSPS.
Hi
30 MHz for both Rx and Tx.
Do you know a transceiver that fits these requirements?
HI olegeorg
As the sample rates are provided not regular one to use.
AD9371 may be possible but request to check clock plan
or ADRV9009 is best suited one but still clock rate has to optimized.
Regards,
SJ
Hi,
Do you think that AD9371 is the best options given that I need rx = 92.16 MSPS and tx = 102.4 MSPS?
ADRV9009 support only integer fractions of (1,2,4 and 8) so it does not fit my application:
Hi olegeorg ,
I am checking on it. Yes, you are right we have limitation with device clock frequency multiple. As it is 9/10 ratio of Rx/Tx which is difficult to go further.
one option we have is either use 2 different devices or do different combination of sample rate and implement the remaining rate match in the Host side.
Please find below snapshot from AD9371 GUI for the suitable combination
Regards,
SJ
Hi
Having two devices are not consider as an option. I think there should be a transciver solution (or ADC and DAC on the same PCB with a FMC connector) that allows setting my wanted sampling rates. Do you have any idea?
Hi,
Any idea?
Hi,
Any idea?
Hi,
Any idea?