KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
ADF5355
Recommended for New Designs
The ADF5355 allows implementation of fractional-N or integer-N phase-locked loop (PLL) frequency synthesizers when used with an external loop filter and...
Datasheet
ADF5355 on Analog.com
AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiverâ„¢ designed for use in 3G and
4G base station applications....
Datasheet
AD9361 on Analog.com
Hi, currently I'm using FMCOMMS5 + zcu102 design. In order for both ad9361 to share the same oscillator reference I added the component adf5355 to the design and to the device tree following the link linux/arch/arm64/boot/dts/xilinx/zynqmp-zcu102-rev10-ad9361-fmcomms5-ext-lo-adf5355.dts at main · analogdevicesinc/linux · GitHub.
However, at the time of receiving it only works at certain frequencies up to 6 GHz. For example, at 2GHz the ad9361 doesn't receive information at all, but around its vicinities it does. This phenomena happens for some frequencies (apparently) without following any pattern. Does anybody know why this happens or someone has bumped into this scenario as well?
Also, using pyadi-iio interface, sometimes port from ad9361-B stop working from execution to execution.
Thanks in advance,
Joaquín.
Hi JoaquinTh ,
Just injecting a tiny question to your discussion: Do you take the RF input signal from a RF signal generator?
I've never used the setup in question, but it sounds like there is a possibility that the PLL is in integer mode. With a PLL frequency setting where you are not getting any input, try dialing the RF generator's frequency up and down to see if there is a frequency nearby that the system is able to receive.
Cheers, heke
Hi JoaquinTh ,
Just injecting a tiny question to your discussion: Do you take the RF input signal from a RF signal generator?
I've never used the setup in question, but it sounds like there is a possibility that the PLL is in integer mode. With a PLL frequency setting where you are not getting any input, try dialing the RF generator's frequency up and down to see if there is a frequency nearby that the system is able to receive.
Cheers, heke
Hi Heke,
No, I'm using the set-up in analog loopback mode before using a RF signal generator.
Greetings,
Joaquín