KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADF5355
Recommended for New Designs
The ADF5355 allows implementation of fractional-N or integer-N phase-locked loop (PLL) frequency synthesizers when used with an external loop filter and...
Datasheet
ADF5355 on Analog.com
AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiverâ„¢ designed for use in 3G and
4G base station applications....
Datasheet
AD9361 on Analog.com
Hi, currently I'm using FMCOMMS5 + zcu102 design. In order for both ad9361 to share the same oscillator reference I added the component adf5355 to the design and to the device tree following the link linux/arch/arm64/boot/dts/xilinx/zynqmp-zcu102-rev10-ad9361-fmcomms5-ext-lo-adf5355.dts at main · analogdevicesinc/linux · GitHub.
However, at the time of receiving it only works at certain frequencies up to 6 GHz. For example, at 2GHz the ad9361 doesn't receive information at all, but around its vicinities it does. This phenomena happens for some frequencies (apparently) without following any pattern. Does anybody know why this happens or someone has bumped into this scenario as well?
Also, using pyadi-iio interface, sometimes port from ad9361-B stop working from execution to execution.
Thanks in advance,
Joaquín.
HI Joaquin567
Thanks for your query.
This looks like some integration issue in linux, if it is happening intermittently then pls check on the version and check initial bootup log if all the devices are initialized successfully.
Also, if you have power or clock issues on the board. we need to check if the PLL clock is locked or not, also similarly check for AD9361 PLL lock status. if you try with internal PLL or some external clock are you seeing this behavior.
Regards,
SJ
Hi, same person with different account. I will delve into the problematic I'm having a bit further.
First of all, I'm using pyadi-iio in order to access the FMComms5 parameters and modify them. In order to configure the adf5355 frequency which will then be distributed to each of the ad9361 I do the following:
ctx = sdr._ctx
adf5355 = ctx.find_device("adf5355")
ch= adf5355.find_channel("altvoltage0",True)
ch.attrs["frequency"].value="4000000000"
After changing the frequency, in the same zcu102 I verify it through:
iio_attr -c adf5355 altvoltage0 frequency
iio_attr -c adf5355 altvoltage1 frequency
And I get:
altvoltage0 = 4000000000
altvoltage1 = 8000000000
Which I understand that is working properly.
Afterwards, I check the PLL status of the adf5355. Since it does not have any attribute to acces to in order to check it is LOCK, I do the following:
cat /sys/kernel/debug/gpio | grep adf5355
gpio-476 ( |adf5355 ) in hi
The second line is the output of the command, which is hi for any given frequenct. Does this output correspond to the PLL LOCK or not?
Other thing I have noticed is that when I execute the commands
iio_reg ad9361-phy 0x247
iio_reg ad9361-phy-B 0x247
which correspodn to the register of the PLL status, both of them return 0x00, but since the frequency and PLL stability is governed by adf5355 this shouldn't matter, or both do have to be locked, which is, 0x01?
Also, I saw in FMCOMMS5 Use ADF5355 as ext LO - Q&A - Support AD9361/AD9363/AD9364 - EngineerZone that the adf5355 wasn't working because of the missing E507 resistor, but in my case it is present in the fmcomms5, could it be another component?
Still. the same keeps happening, the correct functioning of the system depends on the frequency of the adf5355, which shouldn't be happening.
Best regards,
Joaquin.
Hi JoaquinTh ,
Just injecting a tiny question to your discussion: Do you take the RF input signal from a RF signal generator?
I've never used the setup in question, but it sounds like there is a possibility that the PLL is in integer mode. With a PLL frequency setting where you are not getting any input, try dialing the RF generator's frequency up and down to see if there is a frequency nearby that the system is able to receive.
Cheers, heke
Hi Heke,
No, I'm using the set-up in analog loopback mode before using a RF signal generator.
Greetings,
Joaquín
Hi Heke ,
Yes it does, analog devices provides an app called iio-oscilloscope which allows to control FMComms5 parameters and control TX signal. Precisely with this app I could determine that after including adf5355 in the device tree, depending on the LO frequency, the received signal suffers more or less attenuation.
Cheers, Joaquin.
Hi JoaquinTh ,
OK. Thank you.
I assume that the iio-oscilloscope probes the RX baseband signal, which means that it is not possible to tell whether the problem lies in TX or in RX. That information would be extremely useful. You would need to cut the loopback and use a spectrum analyzer and an RF signal generator to test each direction separately.
It is possible that the loopback path is not properly matched.
Cheers, heke