Post Go back to editing

AD9361 BIST IQ data mask confusion

Thread Summary

The user observed that masking C1/2-I in the AD9361 BIST settings results in zero values on the Q data ports (adc_data_q0/adc_data_q1), and vice versa. This suggests a potential issue with the BIST register map (0x3F6) description. The Analog Devices support team is investigating the problem and will provide a solution.
AI Generated Content
Category: Hardware
Product Number: AD9361

I would like to clear this issue that I have with AD9361 and BIST IQ masking.
In picture AD9361_ip_connect_block_diagram.png is block diagram with AD9361 IP core IQ data port adc_data_i0/adc_data_i1 and adc_data_q0/adc_data_q1 connections. In picture VHDL_signal_connection.png is how this ports from AD9361 are connected to internal signals that are then captured with ChipScope.



In picture UG_BIST_regmap.png the UG-671 AD9361 registers for BIST are described.



Pictures CS_mask_C1-I.png shows ChipScope captured signals if C1-I is masked and picture IIO_mask_C1-I.png shows corresponding content of BIST registers when C1-I is checked in IIO Oscillosope.


Pictures CS_mask_C1-Q.png and IIO_mask_C1-Q.png shows the result if BIST C1-Q is masked.


Pictures CS_mask_C1-Q_C2-Q.png and IIO_mask_C1-Q_C2-Q.png shows result if Q is masked on both ports.



What I see is that if C1/2-I is masked, the data that comes out from AD9361 from port adc_data_q0/adc_data_q1 are masked out (zero value). Same swapping is for C1/2-Q data masking, AD9361 port adc_data_i0/adc_data_i1 are masked out (zero value).

I did this test to exclude that real signal IQ data are swapped somewhere in data path up to PC capturing:
If I output a fixed Bist TONE (no IQ masking) and than plot captured IQ data, the captured data is cos/sin plot where I data are leading Q data for 90deg. Additionally the FFT plot of this data shows tone peak frequency on the positive side (+Fs/2) of FFT plot.
Based on this plotting data I assume that AD9361 data on port adc_data_i0/adc_data_i1 are really I data and adc_data_q0/adc_data_q1 are really Q data of captured tone signal. 
If this IQ data would be swapped somewhere in data pipeline, the FFT plot would result with tone peak frequency on the left side (negative side -F2/2).

From above it looks to me that register map description for BIST register 0x3F6 is not correct.
Can someone please help me out from this confusion.

WBR Primoz

Thread Notes

Parents
  • Hi,

    Could you please take a look at this thread and see if clearing the PP RX SWAP IQ bit solves your issue?

    AD9361 I/Q data swap - Q&A - Support AD9361/AD9363/AD9364 - EngineerZone

    Regards,

    Ionut

  • Hi Ionut,

    I have tried the suggested register 0x010 D6 bit which has function "PP Rx Swap IQ" described in UG-673 in Table.11. This bit indeed swaps IQ. But this IQ swapping is not limited to only BIST mode as it is described in solution from link that you provided.Clearing this bit will swap IQ data in general, also(!) for normal RF data capture mode.

    Proposed solution of clearing D6 bit in register 0x010 is kind of workaround in the sense: "If you switch to BIST mode and would like to mask out IQ data via register 0x3F6, than you must first clear D6 bit in register 0x010. But remember to set it again when you switch out of BIST mode."

    So I think that original root of the problem is in bit description in UG-673 for BIST register 0x3F6 D3-"BIST Mask Q data" and D2-"BIST Mask I data".

    From your provided information I can now be pretty sure that the problem is in UG-673. Description for register 0x3F6 IQ masking is not correct. D2 controls Q masking and D3 controls I masking.

    Knowing this can be considered as a solution for me, but original bug will remain in UG-673 documentation.

    WBR Primoz

Reply
  • Hi Ionut,

    I have tried the suggested register 0x010 D6 bit which has function "PP Rx Swap IQ" described in UG-673 in Table.11. This bit indeed swaps IQ. But this IQ swapping is not limited to only BIST mode as it is described in solution from link that you provided.Clearing this bit will swap IQ data in general, also(!) for normal RF data capture mode.

    Proposed solution of clearing D6 bit in register 0x010 is kind of workaround in the sense: "If you switch to BIST mode and would like to mask out IQ data via register 0x3F6, than you must first clear D6 bit in register 0x010. But remember to set it again when you switch out of BIST mode."

    So I think that original root of the problem is in bit description in UG-673 for BIST register 0x3F6 D3-"BIST Mask Q data" and D2-"BIST Mask I data".

    From your provided information I can now be pretty sure that the problem is in UG-673. Description for register 0x3F6 IQ masking is not correct. D2 controls Q masking and D3 controls I masking.

    Knowing this can be considered as a solution for me, but original bug will remain in UG-673 documentation.

    WBR Primoz

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.