Post Go back to editing

Calibration TIMEOUT (0x5E, 0x80) Issue

Thread Summary

The user encountered calibration timeouts/errors during AD9364 initialization using the RM57L843 microcontroller and an FPGA. The issue was resolved by configuring the SPI clock polarity to idle low, as required by the AD9364. The reference clock was 40 MHz, and all power supply rails were stable.
AI Generated Content
Category: Software
Product Number: AD9364

Hi,

We are using the AD9364 RF Agile Transceiver in our project. The SPI interface of the AD9364 is controlled by the RM57L843 microcontroller, while the remaining control and data interface lines are connected to an FPGA.

I have integrated our RM57 SPI driver into the no-OS library by modifying generic_spi.c to use our platform-specific SPI functions.

Current Status

  • SPI communication is working correctly.

  • I am able to successfully read the AD9364 Device ID.

  • Hardware reset of the AD9364 is working.

  • Reference clock is stable.

  • Reference clock amplitude is 0.8v  Vp-p.

  • All power supply rails are stable and within specification.

However, when I call:

ad9361_init(&phy, &init);

the initialization fails with a calibration error. The log shows calibration timeout/errors after the device ID read and reset are completed successfully.

Has anyone encountered calibration failures in this situation? Could this be related to:

  • BBPLL or RFPLL configuration?

  • Reference clock configuration in init.reference_clk_rate?

  • FPGA interface timing?

  • ENSM state transitions?

  • Reset timing sequence?

Any suggestions on what to check next would be greatly appreciated.

[CortexR5] ad9361_reset: by GPIO
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_setup
ad9361_auxdac_setup
ad9361_auxdac_set DAC1 = 0 mV
ad9361_auxdac_set DAC2 = 0 mV
ad9361_gpo_setup
ad9361_set_dcxo_tune : coarse 8 fine 5920
ad9361_set_trx_clock_chain
ad9361_set_trx_clock_chain: 983040000 245760000 122880000 61440000 30720000 30720000
ad9361_set_trx_clock_chain: 983040000 245760000 122880000 61440000 30720000 30720000
ad9361_bbpll_set_rate: Rate 983040000 Hz Parent Rate 40000000 Hz
Calibration TIMEOUT (0x5E, 0x80)
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_clk_factor_set_rate: Rate 240000440 Hz Parent Rate 960001761 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_clk_factor_set_rate: Rate 4294967274 Hz Parent Rate 120000220 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_clk_factor_set_rate: Rate 120000220 Hz Parent Rate 120000220 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_clk_factor_set_rate: Rate 120000220 Hz Parent Rate 120000220 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_clk_factor_set_rate: Rate 60000110 Hz Parent Rate 120000220 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_clk_factor_set_rate: Rate 60000110 Hz Parent Rate 120000220 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_clk_factor_set_rate: Rate 30000055 Hz Parent Rate 60000110 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_clk_factor_set_rate: Rate 30000055 Hz Parent Rate 60000110 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_clk_factor_set_rate: Rate 30000055 Hz Parent Rate 30000055 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_clk_factor_set_rate: Rate 30000055 Hz Parent Rate 30000055 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rssi_setup
ad9361_auxadc_setup
ad9361_rf_port_setup : INPUT_SELECT 0x3
ad9361_pp_port_setup
ad9361_auxadc_setup
ad9361_ctrl_outs_setup
ad9361_set_ref_clk_cycles : ref_clk_hz 40000000
ad9361_clk_factor_set_rate: Rate 80000000 Hz Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_clk_factor_set_rate: Rate 80000000 Hz Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
ad9361_txrx_synth_cp_calib : ref_clk_hz 80000000 : is_tx 0
Calibration TIMEOUT (0x244, 0x80)
ad9361_init : AD936x initialization error

and this is the init parameters

struct ad9361_rf_phy *phy;

AD9361_InitParam init = {
/* Device selection */
.dev_sel = ID_AD9364,

/* Reference Clock */
.reference_clk_rate = 40000000UL,

/* Base Configuration */
.two_rx_two_tx_mode_enable = 0, // AD9364 = 1R1T only
.one_rx_one_tx_mode_use_rx_num = 1, // Use RX1
.one_rx_one_tx_mode_use_tx_num = 1, // Use TX1

.frequency_division_duplex_mode_enable = 1, // FDD mode (recommended)
.frequency_division_duplex_independent_mode_enable = 0,

.tdd_use_dual_synth_mode_enable = 0, // Not needed for FDD
.tdd_skip_vco_cal_enable = 0, // Keep calibration enabled

.tx_fastlock_delay_ns = 0, // Not using fastlock
.rx_fastlock_delay_ns = 0,

.rx_fastlock_pincontrol_enable = 0,
.tx_fastlock_pincontrol_enable = 0,

.external_rx_lo_enable = 0, // Internal LO
.external_tx_lo_enable = 0,

.dc_offset_tracking_update_event_mask = 5, // Recommended default
.dc_offset_attenuation_high_range = 6,
.dc_offset_attenuation_low_range = 5,
.dc_offset_count_high_range = 0x28,
.dc_offset_count_low_range = 0x32,

.split_gain_table_mode_enable = 0, // Normal gain table

.trx_synthesizer_target_fref_overwrite_hz = MAX_SYNTH_FREF, // Use default ref

.qec_tracking_slow_mode_enable = 0, // Normal QEC tracking

/* ENSM Control */
.ensm_enable_pin_pulse_mode_enable = 0, // Use SPI control
.ensm_enable_txnrx_control_enable = 0, // SPI controls ENSM


/* LO Control */
.rx_synthesizer_frequency_hz = 2400000000ULL,
.tx_synthesizer_frequency_hz = 2400000000ULL,
.tx_lo_powerdown_managed_enable = 0,

/* Rate & BW Control */
.rx_path_clock_frequencies[0] = 983040000UL, // BBPLL
.rx_path_clock_frequencies[1] = 245760000UL,
.rx_path_clock_frequencies[2] = 122880000UL,
.rx_path_clock_frequencies[3] = 61440000UL,
.rx_path_clock_frequencies[4] = 30720000UL,
.rx_path_clock_frequencies[5] = 30720000UL, // Sample rate

.tx_path_clock_frequencies[0] = 983040000UL,
.tx_path_clock_frequencies[1] = 245760000UL,
.tx_path_clock_frequencies[2] = 122880000UL,
.tx_path_clock_frequencies[3] = 61440000UL,
.tx_path_clock_frequencies[4] = 30720000UL,
.tx_path_clock_frequencies[5] = 30720000UL,

.rf_rx_bandwidth_hz = 20000000UL,
.rf_tx_bandwidth_hz = 20000000UL,


.rx_rf_port_input_select = 0, // RX1A
.tx_rf_port_input_select = 0, // TX1A

.tx_attenuation_mdB = 10000, // 10 dB
.update_tx_gain_in_alert_enable = 0,

.xo_disable_use_ext_refclk_enable = 0, // Use internal crystal
.dcxo_coarse_and_fine_tune[0] = 8,
.dcxo_coarse_and_fine_tune[1] = 5920,
.clk_output_mode_select = 0, // Disable clock out

/* Gain Control */
.gc_rx1_mode = RF_GAIN_MGC,

.gc_adc_large_overload_thresh = 58,
.gc_adc_ovr_sample_size = 4,
.gc_adc_small_overload_thresh = 47,
.gc_dec_pow_measurement_duration = 8192,

.gc_dig_gain_enable = 0,
.gc_lmt_overload_high_thresh = 800,
.gc_lmt_overload_low_thresh = 704,
.gc_low_power_thresh = 24,
.gc_max_dig_gain = 15,
.gc_use_rx_fir_out_for_dec_pwr_meas_enable = 0,

.mgc_dec_gain_step = 2,
.mgc_inc_gain_step = 2,
.mgc_rx1_ctrl_inp_enable = 0,
.mgc_rx2_ctrl_inp_enable = 0,
.mgc_split_table_ctrl_inp_gain_mode = 0,

.agc_adc_large_overload_exceed_counter = 10,
.agc_adc_large_overload_inc_steps = 2,
.agc_adc_lmt_small_overload_prevent_gain_inc_enable = 0,
.agc_adc_small_overload_exceed_counter = 10,
.agc_dig_gain_step_size = 4,
.agc_dig_saturation_exceed_counter = 3,
.agc_gain_update_interval_us = 1000,

.agc_immed_gain_change_if_large_adc_overload_enable = 0,
.agc_immed_gain_change_if_large_lmt_overload_enable = 0,

.agc_inner_thresh_high = 10,
.agc_inner_thresh_high_dec_steps = 1,
.agc_inner_thresh_low = 12,
.agc_inner_thresh_low_inc_steps = 1,

.agc_lmt_overload_large_exceed_counter = 10,
.agc_lmt_overload_large_inc_steps = 2,
.agc_lmt_overload_small_exceed_counter = 10,

.agc_outer_thresh_high = 5,
.agc_outer_thresh_high_dec_steps = 2,
.agc_outer_thresh_low = 18,
.agc_outer_thresh_low_inc_steps = 2,

.agc_attack_delay_extra_margin_us = 1,
.agc_sync_for_gain_counter_enable = 0,

/* Fast AGC */
.fagc_dec_pow_measuremnt_duration = 64,
.fagc_state_wait_time_ns = 260,

/* Fast AGC - Low Power */
.fagc_allow_agc_gain_increase = 0,
.fagc_lp_thresh_increment_time = 5,
.fagc_lp_thresh_increment_steps = 1,

/* Fast AGC - Lock Level */
.fagc_lock_level_lmt_gain_increase_en = 1,
.fagc_lock_level_gain_increase_upper_limit = 5,

/* Final Settling */
.fagc_lpf_final_settling_steps = 1,
.fagc_lmt_final_settling_steps = 1,
.fagc_final_overrange_count = 3,

/* Final Power Test */
.fagc_gain_increase_after_gain_lock_en = 0,

/* Unlocking */
.fagc_gain_index_type_after_exit_rx_mode = 0,
.fagc_use_last_lock_level_for_set_gain_en = 0,
.fagc_rst_gla_stronger_sig_thresh_exceeded_en = 0,
.fagc_optimized_gain_offset = 5,
.fagc_rst_gla_stronger_sig_thresh_above_ll = 10,
.fagc_rst_gla_engergy_lost_sig_thresh_exceeded_en = 0,
.fagc_rst_gla_engergy_lost_goto_optim_gain_en = 0,
.fagc_rst_gla_engergy_lost_sig_thresh_below_ll = 10,
.fagc_energy_lost_stronger_sig_gain_lock_exit_cnt = 3,
.fagc_rst_gla_large_adc_overload_en = 0,
.fagc_rst_gla_large_lmt_overload_en = 0,
.fagc_rst_gla_en_agc_pulled_high_en = 0,
.fagc_rst_gla_if_en_agc_pulled_high_mode = 0,
.fagc_power_measurement_duration_in_state5 = 8192,
.fagc_large_overload_inc_steps = 2,

.rssi_delay = 1,
.rssi_duration = 1000,
.rssi_restart_mode = 3,
.rssi_unit_is_rx_samples_enable = 0,
.rssi_wait = 1,

.aux_adc_decimation = 256,
.aux_adc_rate = 40000000UL,

.aux_dac_manual_mode_enable = 0,

.aux_dac1_default_value_mV = 0,
.aux_dac1_active_in_rx_enable = 0,
.aux_dac1_active_in_tx_enable = 0,
.aux_dac1_active_in_alert_enable = 0,
.aux_dac1_rx_delay_us = 0,
.aux_dac1_tx_delay_us = 0,

.aux_dac2_default_value_mV = 0,
.aux_dac2_active_in_rx_enable = 0,
.aux_dac2_active_in_tx_enable = 0,
.aux_dac2_active_in_alert_enable = 0,
.aux_dac2_rx_delay_us = 0,
.aux_dac2_tx_delay_us = 0,

.temp_sense_decimation = 256,
.temp_sense_measurement_interval_ms = 1000,
.temp_sense_offset_signed = 0,
.temp_sense_periodic_measurement_enable = 1,

.ctrl_outs_enable_mask = 0x00,
.ctrl_outs_index = 0,

.elna_settling_delay_ns = 0,
.elna_gain_mdB = 0,
.elna_bypass_loss_mdB = 0,
.elna_rx1_gpo0_control_enable = 0,
.elna_rx2_gpo1_control_enable = 0,
.elna_gaintable_all_index_enable = 0,

.digital_interface_tune_skip_mode = 0,
.digital_interface_tune_fir_disable = 0,

.pp_tx_swap_enable = 0,
.pp_rx_swap_enable = 0,
.tx_channel_swap_enable = 0,
.rx_channel_swap_enable = 0,

.rx_frame_pulse_mode_enable = 0,
.two_t_two_r_timing_enable = 0,
.invert_data_bus_enable = 0,
.invert_data_clk_enable = 0,
.fdd_alt_word_order_enable = 0,
.invert_rx_frame_enable = 0,
.fdd_rx_rate_2tx_enable = 0,
.swap_ports_enable = 0,
.single_data_rate_enable = 0, // DDR mode
.lvds_mode_enable = 1, // LVDS
.half_duplex_mode_enable = 0,
.single_port_mode_enable = 0,
.full_port_enable = 1,
.full_duplex_swap_bits_enable = 0,

.delay_rx_data = 0,
.rx_data_clock_delay = 0,
.rx_data_delay = 0,
.tx_fb_clock_delay = 0,
.tx_data_delay = 0,

.lvds_bias_mV = 150,
.lvds_rx_onchip_termination_enable = 1,

.rx1rx2_phase_inversion_en = 0,
.lvds_invert1_control = 0,
.lvds_invert2_control = 0,

/* GPO Control */
.gpo_manual_mode_enable = 0,
.gpo_manual_mode_enable_mask = 0x0,

.gpo0_inactive_state_high_enable = 0,
.gpo1_inactive_state_high_enable = 0,
.gpo2_inactive_state_high_enable = 0,
.gpo3_inactive_state_high_enable = 0,

.gpo0_slave_rx_enable = 0,
.gpo0_slave_tx_enable = 0,
.gpo1_slave_rx_enable = 0,
.gpo1_slave_tx_enable = 0,
.gpo2_slave_rx_enable = 0,
.gpo2_slave_tx_enable = 0,
.gpo3_slave_rx_enable = 0,
.gpo3_slave_tx_enable = 0,

.gpo0_rx_delay_us = 0,
.gpo0_tx_delay_us = 0,
.gpo1_rx_delay_us = 0,
.gpo1_tx_delay_us = 0,
.gpo2_rx_delay_us = 0,
.gpo2_tx_delay_us = 0,
.gpo3_rx_delay_us = 0,
.gpo3_tx_delay_us = 0,

/* Tx Monitor Control */
.low_high_gain_threshold_mdB = 37000,
.low_gain_dB = 0,
.high_gain_dB = 24,

.tx_mon_track_en = 0,
.one_shot_mode_en = 0,
.tx_mon_delay = 511,
.tx_mon_duration = 8192,

.tx1_mon_front_end_gain = 2,
.tx2_mon_front_end_gain = 2,

.tx1_mon_lo_cm = 0x3F,
.tx2_mon_lo_cm = 0x3F,

.spi_param = spi_init,
.gpio_resetb = gpio_reset,

.ad9361_rfpll_ext_recalc_rate = NULL,
.ad9361_rfpll_ext_round_rate = NULL,
.ad9361_rfpll_ext_set_rate = NULL,

.rx_adc_init = NULL,
.tx_dac_init = NULL,
};

Thanks,

Regards,

Veerappan P.

Edit Notes

The wrong reference clock amplitude was previously updated as 1.2v Vp-p. Now it corrected to 0.8v Vp-p
[edited by: Veerappan at 8:38 AM (GMT -5) on 23 Feb 2026]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.