Hello Team,
I referred to the FMCOMMS5 validation documentation, specifically the FMCOMMS5 Phase Synchronization page on the Analog Devices Wiki ( FMComms5 Phase Synchronization [Analog Devices Wiki] ). The reference mentions validation using a 30.72 MSPS sampling rate. Could you please confirm whether the ZCU102 supports operation with the FMCOMMS5 at a 61.44 MSPS sampling rate and an RX LO frequency of 2400 MHz? If supported, kindly let us know if there are any specific configuration requirements or recommended settings to achieve stable operation at this sampling rate.