Post Go back to editing

Issue with AD9364 Filter Wizard 24.1.1 – Buttons Greyed Out

Category: Software
Product Number: AD9364
Software Version: 24.1.1

Hi All,

I’m currently working with the AD9364 on a custom board using the non-OS drivers. I’m trying to design a low-pass filter using the AD9364 Filter Wizard (version 24.1.1), but I’m encountering some issues.

The main problem is that several buttons in the tool are greyed out, including the ones for exporting coefficients to the filter and to the non-OS driver. I also tried using the default LTE15 filter example, but the issue persists—the buttons remain inactive.

I’ve attached a short video demonstrating the problem. Could you please take a look and let me know if there’s a workaround or solution?

Best regards,
Sachin

  • HI  

    Looks like some glitch in filter wizard. In the filter design, initially you start with Transmit and then you go for receive filter design. All the options are enabled in my case with these steps.

    Kindly note, whenever you change the Device settings, it would be good if you start with Transmit filter design and then go for Receive filter design.

    Regards,

    SJ