Post Go back to editing

Spike over the Received IQ

Category: Software
Product Number: AD9364

Hi Team ,

I'm using a custom board based on the Spartan-7 FPGA interfaced with the AD9364 transceiver. In this setup, an external microcontroller acts as the SPI master, responsible for configuring the AD9364 registers using the Analog Devices no-OS driver framework. The FPGA's role is limited to receiving and forwarding IQ data.

However, we have observed intermittent anomalies in the received IQ data. Specifically, spurious spikes occasionally appear on the IQ waveform, as shown in the attached image. Notably, these spikes disappear after performing a power cycle, after which the IQ data appears clean and stable. This behavior is consistent across both RF loopback tests on the same board and during transmission between two separate boards.

                                                                                                  

Could you please provide the potential causes of this issue, along with recommended methods to prevent it?

Regards,

PARAS ADT Blr

Thread Notes

Parents Reply Children
  • HI  

    Just to ensure that, what is the switching Freq applied in the power supply.?

    Pls change the Freq and see the behavior.

    Does the spike Freq changing with power supply ?

    if you terminate the Rx port with 50ohm and then also are you observing any spikes in Rx Data.?

    Regards,

    SJ

  • Hi  ,

    When I terminate the Rx port with 50 Ω, I still observe spikes in the received data.

    Regarding the power-supply switching frequency, I was advised to use the MAX77511, whose nominal switching frequency is approximately 1 MHz.

    I also evaluated a different PMIC and varied its switching frequency. However, I continue to observe the same spikes, with no change in the spike occurrence frequency, even after modifying the power-supply switching frequency.

    Please let me know if further measurements or checks are required.

    Regards,

    PADT

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.