Post Go back to editing

Spike over the Received IQ

Category: Software
Product Number: AD9364

Hi Team ,

I'm using a custom board based on the Spartan-7 FPGA interfaced with the AD9364 transceiver. In this setup, an external microcontroller acts as the SPI master, responsible for configuring the AD9364 registers using the Analog Devices no-OS driver framework. The FPGA's role is limited to receiving and forwarding IQ data.

However, we have observed intermittent anomalies in the received IQ data. Specifically, spurious spikes occasionally appear on the IQ waveform, as shown in the attached image. Notably, these spikes disappear after performing a power cycle, after which the IQ data appears clean and stable. This behavior is consistent across both RF loopback tests on the same board and during transmission between two separate boards.

                                                                                                  

Could you please provide the potential causes of this issue, along with recommended methods to prevent it?

Regards,

PARAS ADT Blr

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.