hello.
I have degign a board with zynq010 and ad9363.
My problem is when in cmos mode. the ad9363 works fine.
in lvds mode.
the rx path works fine,I check it by send a signal from outside and the rx signal looks ok :

but when I connect rx1 to tx1. use dds to generate a sine wave with tx1.
the receive signal become bad.

my hardware condition is:
zynq software platform: plutosdr fimware.
vdd digital voltage: 1.8v.
zynq bank voltage: 1.8v.
I set the adi,digital-interface-tune-skip-mode to 2 ,because when set to 0,It canot pass .
any suggestion??