Our application is TDD 2T/2R ,We would like to monitor Tx power and Rx signal.
Can you provide bilock diagram for Tx Monitor and RSSI?
AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiverâ„¢ designed for use in 3G and
4G base station applications....
Datasheet
AD9361 on Analog.com
Our application is TDD 2T/2R ,We would like to monitor Tx power and Rx signal.
Can you provide bilock diagram for Tx Monitor and RSSI?
TX monitor function is used to measure RSSI of TX.
Are you planning to use TX monitor as RX port? You can use TX monitor port as RX but it will have limited dynamic range, no LNA, no AGC.
Refer to the below block diagram from UG:
TX monitor function is used to measure RSSI of TX.
Are you planning to use TX monitor as RX port? You can use TX monitor port as RX but it will have limited dynamic range, no LNA, no AGC.
Refer to the below block diagram from UG:
Thanks.Does AD9361 has DPD function?Which parts has DPD function?
No, this chip doesnot support DPD. DPD applications are supported in ADRV9375,ADRV9009, ADRV9026.