Post Go back to editing

Balun OR transformer

Category: Datasheet/Specs
Product Number: AD9361

The AD-FMComms3-EBZ use the TCM1-63AX+ transformer of choice. but configuration option for AD9361 list of alternative baluns are below:

Can I use baluns to replace TCM1-63AX+ directly or need to additional matching circuit ?

TCM1-63AX+ is 50/50ohm,but following baluns some with 50/100 ohm.I am confuse.

TDK 350 HHM1591D1 50/100 100pF
TDK 900 HHM1564A4 50/200 100pF
Johanson 1450 1450BL15A200E 50/200 20pF
Johanson 1600 1600BL15B050E 50/50 20pf
Anaren 1631 BD1631J50100A00 50/100 18pF
Johanson 2450 2450BL15B200E 50/200 9pF
Johanson 2450 2450BL15B050E 50/50 18pF
Hitachi 3000 ESLT-S370KBI 50/50 10pF
Johanson 5400 5400BL15K050E 50/50 10pF
Hitachi 5000 ESLT_S540E 50/50 10pF

Transmit Balun

Manufacturer Frequency (MHz) Balun number Impedance
TDK 350 HHM1591D1 50/100
Johanson 900 0900BL15C050E 50/50
Johanson 1600 1600BL15B050E 50/50
Johanson 1600 1600BL15B050E 50/50
Johanson 1850 1850BL15B050E 50/50
Johanson 2450 2450BL15B050E 50/50
Johanson 3700 3700BL15B050E 50/50
Johanson 5400 5400BL15K050E 50/50
Johanson 5400 5400BL15K050E 50/50


Update text
[edited by: RaySun at 11:19 PM (GMT -5) on 19 Nov 2024]