Hi
I am using ADRV9364 board with ADRV1CRR-BoB. I am running the no-os. When I run the no-os in default settings, I see clean Rx data. but when I change the mode to MGC and give a small gain (i.e. 0-30, that does not cause overflow) then the signal at the Rx has some noise in it.
I want to know how can I remove the noise and where is it coming form.
MGC 20:

MGC 5:

The second issue is that the here adc and dac valid is high once every 1 cycle (1 valid in 2 cycles). But with AD9361, I have observed that the adc and dac valid is high once every 3 cycle (1 valid in 4 cycles).
A clean picture with default AGC enabled. Here the signal received at the adc is clean: