Post Go back to editing

AD9361 maximum CLK_OUT frequency

Thread Summary

The user wants to use the CLK_OUT pin of the AD9361 to output an 80 MHz clock, but the CMOS mode is limited to 61.44 MHz. The final answer confirms that CLK_OUT cannot exceed 61.44 MHz in CMOS mode. An alternative is to use the REF_CLK input directly, which can be scaled to 80 MHz after a *2 scaling. If CLK_OUT is not used, it can be left floating.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD9361

I want to use the CLK_OUT pin of the AD9361 as an input to my FPGA.  I am using an external clock input of 80 MHz, and I would like that 80MHz to come out of the CLK_OUT pin (i.e. set CLKOUT select of Table 9 in UG-671 to 000).  However, in UG-570 that the clock frequency must be less than 61.44MHz.  Does this mean the CLOCK_OUT is clamped to 61.44MHz?  It won't show me a buffered copy of my 80 MHz clock input? 

Thanks,

- Jon

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.