Hi, i am using antADR and trying to use Ad9361 in MIMO mode with both tx and rx enabled. I have modified the devicetree file to enable 2tx,2rx mode, and used that in the BOOT partition of SD card. My belief is that by default Tx1 and Rx1 port of the SDR is enabled and working, but if i want to use Tx and Rx diversity i need to enable both tx and rx via commands. Can someone share, if my thinking is correct and if yes what should be the commands to do this?
Thanks and regards
Nitin