Hi everyone,
We are having trouble getting spurs in the desired band—let's say, the 5 MHz band—while using the specially made AD9364 board for our project.
Frequency of tone: 2.5 MHz
LO: 3 GHz
Observed in the spectrum analyzer (SA)
Up-Band: -3 dBm at 3.0025 GHz
Spurs: -50 dBm carrier offset of 186 KHz (Delta Marker)
(See the photo attached.)
We verified that the power supply switching frequency was not the cause of the spur and followed the layout guidelines as advised by the analog devices.
The reference clock source is operating at 40 MHz, and we used a spectrum analyzer to make sure we weren't receiving any undesirable frequencies.
We are seeing the same issue in four developed boards.
Please advise how if we can reduce the spur