Dear ADI,
I want to refer to the reference design of ADRV9361-Z7035 for use, but found that the official website only has this schematic diagram and BOM. Where can I get the PCB layout file of ADRV9361-Z7035?
AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiverâ„¢ designed for use in 3G and
4G base station applications....
Datasheet
AD9361 on Analog.com
Dear ADI,
I want to refer to the reference design of ADRV9361-Z7035 for use, but found that the official website only has this schematic diagram and BOM. Where can I get the PCB layout file of ADRV9361-Z7035?
LeonXue - Moved from FPGA Reference Designs to Design Support AD9361/AD9363/AD9364. Post date updated from Wednesday, February 21, 2024 9:33 AM UTC to Thursday, February 22, 2024 10:39 AM UTC to reflect the move.
Hi,
I will get in touch with the team and come back as soon as I have an answer, but most likely it is not made available for the public if it can't be found neither on wiki nor on analog.com.
Best regards,
Iulia
Hi,
I will get in touch with the team and come back as soon as I have an answer, but most likely it is not made available for the public if it can't be found neither on wiki nor on analog.com.
Best regards,
Iulia
Hi iuLia,
Thanks for your reply.
I would like to get some hardware design suggestions for the AD9361 in high-density design from the source design file of the ADRV9361-Z7035.
Or is there an HW Design guide? I can refer to some key signal design considerations.
You can refer to the "POWER SUPPLY AND LAYOUT GUIDE" section in UG to get information about the layout guidelines.
Below links has the mechanical drawing for SOM board and the layout brd file for the breakout board
https://wiki.analog.com/resources/eval/user-guides/adrv936x_rfsom/hardware
https://wiki.analog.com/resources/eval/user-guides/pzsdr/carriers/brk
Hi,
Could you please provide the link to the UG that includes"POWER SUPPLY AND LAYOUT GUIDE"section?
I don't find the relevant content in the link you provided.
https://wiki.analog.com/resources/eval/user-guides/adrv936x_rfsom/hardware
https://wiki.analog.com/resources/eval/user-guides/pzsdr/carriers/brk
BR