Post Go back to editing

Getting started with AD-FMCOMMS3-EBZ with Xilinx Zynq 7000 ZC702 Evaluation Board on Windows

Thread Summary

The user is trying to build HDL for the AD-FMCOMMS3-EBZ with the Xilinx Zynq 7000 SoC ZC702 Evaluation Board on Windows. The final answer directs the user to a specific thread for further guidance. Accompanying answers suggest using Linux or No-Os drivers, with detailed steps for No-Os drivers and links to relevant Analog Devices wikis for Linux setup and IIO GUI usage.
AI Generated Content
Category: Software
Product Number: AD-FMCOMMS3-EBZ

I can't understand how to get started with using AD-FMCOMMS3-EBZ with my Xilinx Zynq 7000 SoC ZC702 Evaluation Board. Until now I was using Vivado to program my Xilinx Zynq 7000 SoC ZC702 Evaluation Board but now I also want to use the AD-FMCOMMS3-EBZ through FMC connection. I have seen SD boot solutions but it is not what I want. I want to be able to program AD-FMCOMMS3-EBZ on windows. Please someone help me.

Parents Reply
  • Please tell me how can I Build HDL in Windows. Actually I am using Vivado on Windows to program my Xilinx Zynq 7000 SoC ZC702 Evaluation Board. So I want to be able to use the AD-FMCOMMS3-EBZ with Xilinx Zynq 7000 ZC702 Evaluation Board on Windows itself. I understand that I need to build HDL for that but to use the 'make' command etc I require would require a Windows Subsystem for Linux (WSL) but when I am trying to use 'make' then it expects the Vivado files to be in Linux format. I don't understand how can I BUILD HDL in Windows. Please Help. Thank you.

Children
No Data