Hello everyone:
I want to make the rf sync between the two ad9361s in fmcomms5. but it seems the adf5355 does not work properly.
Followed with the wiki, zynq-zc706-adv7511-ad9361-fmcomms5-ext-lo-adf5355 is configured as device.dtb.
Power on the board, and use IIO to test the board, configuring AD9361 use External TX LO, capture no sin wave in the RX channel; but if I uncheck the External TX LO option, rx gets perfect signal.
Followed by AD9361 high performance, highly integrated RF Agile Transceiver Linux device driver [Analog Devices Wiki],
root:/sys/bus/iio/devices/iio:device1> cat out_altvoltage0_RX_LO_frequency
try to use command to config adf5355, but the command get responce with: Device or resource busy
I checked the ADF5335 output RFOUTA & RFOUTB, no LO is generated; and checked the VVCO, turned out to be about 0.8V(should be 4.75V-5.25V according to adf5355 user guide);
FMCOMMS5-EBZ schematic shows that VVCO is generated by ADM7150ARDZ-5.0 (E507), but E507 is not connected;
AD-FMCOMMS5-EBZ User Guide [Analog Devices Wiki
so what should I do to get FMCOMMS5 working well with external LO(adf5355)? should I connect E507?
Edit Notes
change subject[edited by: ivory at 4:27 AM (GMT -5) on 17 Jan 2024]