Post Go back to editing

Regarding the multiple AD9361 reference clock input using 1:8 clock divider

Category: Hardware

Hello support team,

We are planning to use 8 AD9361 boards whose reference clock will be coming from the external environment. I am planning to use 1:8 clock divider which can take sine wave input and generate 8 LVCMOS outputs which further can be provided to 8 AD9361 boards. 

Is above method recommended and suitable option to provide external clocks to multiple AD9361 boards?

Parents Reply Children